Introducing the latest cost-effective door entry range that doesn’t compromise on security or style
Suitable for all requirements from end users to specifiers of the largest developments, Legrand has refreshed and expanded its Bticino Classe 100 range.
![Bticino Classe 100, door entry system, two wire installation, residential, door entry kits](/sites/g/files/ocwmcr866/files/styles/news_teaser_1440x360/public/2023-03/bticino-classe-100-thumbnail1.jpg?itok=fry4FpAL)
Suitable for all requirements from end users to specifiers of the largest developments, Legrand has refreshed and expanded its Bticino Classe 100 range.
With products to suit a variety of buildings, the Classe 100 range equips developers with affordable door entry solutions at every level. The standard two wire installation, across the stylish range means internal units can be easily installed into new developments as well as providing a quick and simple upgrade to be retrofitted in existing dwellings.
A cost-effective range that offers a multitude of benefits such as video feedback and connectivity with smartphones, Classe 100 provides an economical upgrade to door entry systems. Once installed, both the video and audio interfaces provide end users with brilliant functionality.
The hard keys to answer and hang up make for more positive engagement and simplicity of use, whereas the configurable keys allow for personalised, convenient accessibility for every occupant. For added ease of use, the handsets light and flash the appropriate buttons when in use, helping to guide the user and preventing the need to refer to a manual. On top of this, the 100X model enables end users to quickly and easily connect the handsfree unit to their smartphone for increased convenience and security.
Also available in a variety of kits to suit a number of applications, Classe 100 can be quickly implemented to suit a range of new and existing premises, such as schools, hospitals and reception areas as well as residential properties.
Richard Hopkins, Lead Marketing Manager for Legrand’s wiring devices business unit, said: “With the Bticino Classe 100, we seek to offer customers a complete and affordable range that suits any number of requirements and allows them to provide end users with an array of easy-to-use functions. Bringing together economy and style, the range is easy to install thanks to the straightforward two wire installation and, once in place, provides any modern home with great functionality and security.”