Introducing the Nuvo P4300, a multi-zone, rack mounted player

12/04/2017

ShareThis

Legrand, the global specialist in electrical and digital building infrastructures, is proud to announce the launch of its Nuvo P4300 Player, the newest rack mounted model to its Nuvo Player Portfolio range. The most powerful, efficient unit yet, the P4300 boasts simplified installation and diagnostics, with a backlit touch screen display.

Designed by audiophiles for installation by professionals, the three source, three amplifier design enables three independent sources of audio content to be played simultaneously in three rooms.

The P4300 allow users to access music from popular streaming services, including Spotify, TuneIn, Napster, Deezer and SiriusXM, as well as from content stored on networked computers, iOS and Android portable devices. Class D amplifiers deliver the highest quality audio with 110 Watts of power that remains consistent when set to 4, 6 or 8 ohm through the app during set up.

Commenting on the launch, Richard Hayward, Lead Marketing Manager for Legrand UK and Ireland’s Wiring Devices business said: “The P4300 delivers the best professional whole home audio system yet. It pairs the experience of the users’ music, when and where they want it, with incredible power and clarity. Offering a rack mounted solution that packs multiple amps into a single space, a cooler running unit and the added value of the backlit touch screen for gauging diagnostics, the P4300 is ideally suited to the professional integrator, delivering customers the experience they are looking for.”

The player’s backlit touch screen display shows system status and zone name in addition to system configuration information to aid installation. All line inputs and line outputs use a combination 3.5mm analog/Toslink connection and the unit’s side-mounted heat sinks, allow convenient single-space rack mounting to conserve space and increase installation flexibility in the rack.