Adapting and Growing to Changing Customer Needs

21/03/2016

ShareThis

Bringing simplicity and style to the fore, the Equinox range of touch screen control units, from Legrand’s Vantage range of home automation systems, feature a high level of functionality with tailored control and automation technologies for the ultimate personalised home environment.

Now featuring increased widgets and improved definition, the Equinox range offers a modern interface that can be controlled on the go, via a smart phone app.  Modern interfaces combined with powerful InFusion Controllers seamlessly integrate subsystems and enhance the user experience through the creation of individual profile settings.

The touch screen range is intuitive, easy to use and has been designed with the end user in mind, incorporating both light and presence sensors they can be programmed to respond to ambient light and/or detect the user so that the display is always visible, even in darkness.

The Vantage Equinox 73 provides a three-layer user interface, via a 7” LCD touchscreen. Via this large screen, users have the ability to view three widgets at any one time with ultimate control over their environment through the ability to edit and create new scenes. The touch screen unit includes twelve widgets, including lighting, climate, multi-zone audio, cameras, security, and audio/visual.  

The Vantage Equinox 41 has a 4” black glass to edge LCD touch screen offering a slim line alternative to the Equinox 73. What really sets the Equinox 41 LCD touch screen apart from any other, is the addition of user profiles to create an entirely unique user experience. End users also have the ability to schedule, edit, and prioritise the control functions that matter most to them for the ultimate user experience.